Lietuva - Pažymėti Lietuva

„Incoterms“:DDP
Visos kainos nurodytos su pasirinktų siuntimo metodų muito mokesčiais.

Patvirtinkite pasirinktą valiutą:

Eurai
Nemokamas siuntimas daugumai užsakymų, kurių vertė viršija 75 € (EUR).

JAV doleriai
Nemokamas siuntimas daugumai užsakymų, kurių vertė viršija $90 (USD).

Bench Talk for Design Engineers

Bench Talk

rss

Bench Talk for Design Engineers | The Official Blog of Mouser Electronics


A DIY Starting Guide with the Arduino 101 Warren Miller
I have been toying with the idea of diving into the Do It Yourself (DIY) and Maker communities, well maybe more like getting my toe in the water, for a while now, but I just couldn’t find the right project to get started. Then just a few weeks ago I saw the Arduino 101 (Genuino 101 outside the U.S.) and was intrigued by this ‘upgrade’ of the familiar Arduino platform using the low-power Intel Curie™ module.

Tesla Fails to Power the World without Wires Barry Manz
All the hoopla about wireless charging doesn’t hold a candle to what Nikola Tesla had in mind: Providing alternating current through the ground and air and into the world’s products, eliminating transmission lines. If this sounds like fantasy, it indeed turned out to be, but the story of his scheme makes interesting reading.

Walking Ham: A Day in the Life of a “Walking Dead” Amateur Radio Operator Mike Parks
“CQ CQ CQ. This is November One Hotel November Papa. Anyone got their ears on?” I ask the ether. Still, nothing but static. It’s been like this for months now. My stomach is grumbling but my desire to find someone, anyone, is too strong to breakaway from my radio. Not to mention the fact that those roaming monsters scare the heck out of me. Leaving the relatively safe confines of my ham shack is decidedly unappealing except for the annoying little fact that my food supplies are running low. Very low.

The Internet of Controlling Things Warren Miller
The ability to track energy use on almost a device-by-device basis and use energy when it is least expensive is another potential for significant savings. Controlling things seems to be a compelling application for the Internet of Things.

Herd Mentality, Showing a New Way Forward Caroline Storm Westenhover
Back in May 2015, Tesla released the Tesla Power Wall a 7kWh home battery. The idea being that it can be connected to the DC bus in a home and charge from renewables, mainly solar panels and wind turbines, when the production is high but the use is low. Later, they can be discharged during the evening peak times when load demand exceeds supply.

Truly “Wireless” Wireless Charging Emerges Barry Manz
Wireless charging has been less than a spectacular success. Competing (that is, incompatible) standards, a slow reception by smartphone manufacturers, and RF-inhibiting aluminum phone housings and protective cases have resulted in a slow adoption rate by consumers. However, while the prime players have been battling each other, two companies have come up with solutions that eliminate the need for the inductive coils, magnetic resonance, charging pads, and mats that are required by other techniques. Intrigued?

Suddenly Self-Aware AI Making Itself Smarter By The Nanosecond: What Could Go Wrong? Arden Henderson
The "technological singularity" is almost here. No, really. Well, maybe not. The technological singularity is the event where true artificial intelligence comes into being, self-aware, and begins recursive self-improvement by creating entities better than itself. That's one way to put it.

Powered On: The Advancements in Portable Power Justin Risedorf
I dread the beep my phone makes when it’s at the end of its charge. Not because I’m uncomfortable without my phone being on at all times, but because, of course, it always seems to die right when I need it most. I’m using my phone’s navigation to drive through some unfamiliar part of town when it’s dark and rainy and I’m almost out of gas and – beep – my phone is about to die.

All Authors

Show More Show More
View Blogs by Date

Archives