Mouser Press Room
Mouser Facebook Mouser Twitter Mouser RSS Feed Mouser YouTube Channel Mouser Google+ Mouser LinkedIn Mouser Subscription Center Mouser Blog
Mouser Press Room
New Product Announcement

 

NXP's S32V234 Vision and Sensor Fusion Processor, Available from Mouser, Delivers 64-bit Processing for ADAS Applications

January 16, 2018 - Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, now offers the S32V234 vision and sensor fusion processor from NXP Semiconductors. The S32V234 is designed to support safe computation-intensive applications in vision and sensor fusion applications, including Advanced Driver Assistance Systems (ADAS), front camera systems, pedestrian and object recognition, surround view, and machine learning.

The NXP S32V234 processor, available from Mouser Electronics, combines a robust, heterogeneous mix of CPU, GPU and image processors to deliver high-performance processing, vision acceleration, and security features. The processor integrates four Arm® Cortex®-A53 cores running at up to 1 GHz with a NEON coprocessor and an Arm Cortex-M4 CPU. The Cortex-M4 allows automotive operating systems to interface with external devices separate from the Cortex-A53 CPU.

The S32V234 processor offers 4 MBytes of on-chip system RAM and two 32-bit DRAM controllers with support for LPDDR2/DDR3/DDR3L, all with ECC memory. For image processing and vision capabilities, the device includes dual APEX-2 vision accelerators, a GC3000 3D GPU with surround-view support, MIPI CSI2 and parallel image sensor interfaces, and an embedded image signal processor. The S32V234 also offers an impressive array of connectivity features, including Gigabit Ethernet, Zipwire serial interface, dual CAN-FD interfaces, dual-channel FlexRay communication, and a PCI Express (PCIe) lane.

The S32V234 processor provides a wealth of security capabilities, including an on-the-fly AES decryption engine (OTFAD) and a Cryptographic Service Engine (CSE) that meets Secure Hardware Extension (SHE) protocol specifications. The device also features automotive safety compliance capabilities developed through NXP's SafeAssure™ program, which helps manufacturers achieve system compliance with ISO 26262 and IEC 61508 functional safety standards.

The S32V234 processor is supported the SBC-S32V234 Vision Prototype Kit, which offers options for Linux (Yocto) and AutoSAR operating systems. The SBC-S32V234 kit is supported by a complete series of enablement tools and the S32 Design Studio integrated development environment (IDE).

To learn more about the S32V234 processor, visit www.mouser.com/nxp-s32v234-processor. For more information on the SBC-S32V234 Vision Prototype Kit, go to www.mouser.com/nxp-s32v234.


With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 4 million products from over 700 manufacturers. Mouser offers 22 support locations around the world to provide best-in-class customer service and ships globally to over 550,000 customers in 170 countries from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.

Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.



Further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
For press inquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com
Back to Press Room