New at Mouser: Vishay AEC-Q200 IHPT-A Haptic Feedback Actuators for Automotive, Industrial and Consumer Applications

Pranešimas apie naują produktą

Susisiekite su mumis


May 13, 2025Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now shipping the new AEC-Q200 IHPT-A haptic feedback actuators with an Immersion corporation license from Vishay Intertechnology, Inc. The AEC-Q200 IHPT-A actuators feature high force, High Definition (HD) vibrations for clear tactile feedback in noisy environments for consumer, medical, and industrial LCD displays, touchscreens, touch switches, button control and automotive applications.

The Vishay AEC-Q200 IHPT-A haptic feedback actuators, available from Mouser, streamline the design-in process with immersion licenses, eliminating the need to purchase a separate license to implement sophisticated haptic effects. Vishay expands its lineup of IHPT solenoid-based haptic actuators featuring Immersion Corporation licenses with four new AEC-Q200 qualified devices for automotive applications, including dashboards, touchscreens, and center consoles. These actuators feature two-piece magnetic solenoid construction in four sizes (29 × 21mm to 44 × 37mm), with mounting holes comprised of a stationary "U" core and moving "I-bar" for easy implementation. Maximum output force varies from 25 to 120 Newtons depending on size.

The AEC-Q200 IHPT-A devices drive up to a 0.5kg load to 6g of acceleration with a 12V, 5ms pulse, delivering high force and vibration capability for clear, high definition (HD) tactile feedback. The low nominal 12V operation of the automotive IHPT-A devices eliminates the need for the additional high voltage circuitry required by piezo actuators and provides significant advantages over linear resonant, linear wideband, and eccentric rotating mass actuators while reducing component height and delivering higher force.

To learn more, visit https://www.mouser.com/new/vishay/vishay-ihpt-haptic-feedback-actuators/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

About Vishay

2026 - Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.®