Now at Mouser: Taoglas' MA8010 10-in-1 GNSS, Wi-Fi, and 5G/4G Antenna for Next-Generation Routers and Gateways
May 16, 2024 – Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the MA8010 10-in-1 antenna from Taoglas. The MA8010 is a GNSS, Wi-Fi®, and 5G/4G combination antenna designed for use with next-generation routers and gateways. The MA8010 antenna is ideal for emergency and first responder vehicles, electric vehicle chargers, smart industry applications, and private Long-Term Evolution (LTE) networks.
The Taoglas MA8010 10-in-1 antenna, now available at Mouser, combines one dual-band GNSS L1/L5 antenna, four high-efficiency 5G/4G wideband cellular antennas, and five tri-band Wi-Fi antennas into a single unit. The antenna's 600MHz to 6000MHz frequency range ensures enhanced connectivity across a variety of applications. The Taoglas MA8010 antenna features an operating temperature range of -40°C to +85°C and is dust-tight and water-resistant, making it a suitable choice for use in harsh environments.
The MA8010 antenna is smaller than the market standard for 10-connection products, measuring just 350 mm × 70 mm × 39 mm. The small form factor means the MA8010 can be mounted on vehicle roofs and used on various NEMA cabinets. Custom cables and connectors are available for flexible installation and increased compatibility.
To learn more about the MA8010 10-in-1 antenna, visit https://www.mouser.com/new/taoglas/taoglas-10-in-1-screwmount-antennas/.
2026 - Taoglas is a leading provider of antennas, advanced IoT components, and custom design services that help customers navigate complex RF and wireless systems and bring connectivity solutions to market on time, the first time. Since its foundation in 2004, the global company remains committed to continuous innovation, proactive customer service, and trusted quality that delivers long-term peace of mind to customers and colleagues, creating time and space to work together to advance global connectivity.