Mouser Equips Electronic Design Engineers with the Latest Sensor Technologies with Online Resource Center

Pranešimas apie naują produktą

Susisiekite su mumis


Visit Mouser's sensor resource center
Visit Mouser's sensor resource center

September 23, 2025Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, provides today's electronic design engineers with the latest knowledge in sensor technology with its extensive online hub. The evolution of semiconductors and microelectromechanical systems (MEMS) into smaller, more affordable, and reliable components has been a key enabler for modern technology. This has allowed sensors to be seamlessly embedded into almost every device and system, driving the growth of the Internet of Things (IoT) and making advanced data collection more accessible across all industries.

For example, in healthcare, sensors improve advanced diagnostic tools, enable continuous patient monitoring, and support cutting-edge wearables for personal health management. This same technology is transforming agriculture, like in connected cow systems, where sensors and AI provide real-time data to optimize herd health. Additionally, sensors are pushing boundaries in research with LiDAR-equipped drones in marine biology that can accurately evaluate whales' health. Engineers developing these applications can leverage innovative platforms that combine powerful capabilities with compact designs, simplifying the creation of new applications. By merging advanced hardware and streamlined development tools, the engineering community can rapidly prototype and deploy the next generation of sensor-driven applications.

Mouser's sensor content hub offers an extensive collection of articles, blogs, eBooks, and product information from Mouser's technical experts and leading manufacturing partners. In a recent eBook with onsemi, Engineering the Future: The Sensors and Systems Powering Modern Mobile Robots, readers explore a range of sensing technologies, such as cameras and time-of-flight sensors, that enable autonomous mobile robots. The eBook helps engineers understand how each sensor works individually and how they integrate to create a cohesive system. The hub is a valuable resource for engineers seeking to stay ahead of the evolving sensor landscape and build advanced connected systems.

Mouser stocks the industry's widest selection of sensor products and solutions, including the following:

  • The CY8CPROTO-040T-MS multi-sense prototyping kit from Infineon Technologies demonstrates the capacities of fifth-generation CAPSENSE™ technology, including touch-sensing performance and low-power operation with always-on sensing. This kit is split into a control board and multiple daughter boards. It includes a PSOC™ 4000T multi-sense control board, an inductive keypad-4 expansion board, an inductive keypad-2 expansion board, and a liquid-level sensor expansion board.
  • The IQS9150 and IQS9151 ProxSense® sensors by Azoteq are configurable trackpad devices suitable for numerous design variations and requirements. These sensors feature multitouch high-performance (linearity, accuracy, and low-noise) trackpad outputs, integrated snap button options, and an on-chip gesture recognition engine. They feature best-in-class sensitivity, signal-to-noise ratio, and automatic tuning of electrodes.
  • The Mira050 NIR enhanced global shutter image sensors from ams OSRAM are compact 0.5MP near-infrared enhanced global shutter image sensors developed for 2D and 3D consumer and industrial machine vision applications. The sensors have a small 2.79µm pixel size with high sensitivity resulting from state-of-the-art BSI technology. The Mira050 has a MIPI CSI-2 interface, enabling easy interfacing with many processors and FPGAs.
  • The SCH16T-K10 6-DOF sensor by Murata Electronics is a combined high-performance 3-axis gyroscope and 3-axis accelerometer. The gyroscope measurement range is selectable in applications from ±2000°/s down to ±1000°/s, while the accelerometer measurement is selectable from ±160m/s2 down to ±15m/s2. The angular rate and accelerometer sensor elements are based on 3D-MEMS technology, and the signal processing is operated by a signal mixed-signal ASIC.

To learn more, visit https://resources.mouser.com/sensor/. For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.