Mouser Now Stocking EliteSiC Silicon Carbide Solutions from onsemi

Pranešimas apie naują produktą

Susisiekite su mumis


March 20, 2023 – Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, is now stocking the EliteSiC silicon carbide (SiC) family of solutions from onsemi. The EliteSiC portfolio includes diodes, MOSFETs, IGBT and SiC diode Power Integrated Modules (PIMs), and AEC-Q100-qualified devices. These devices are optimized to provide reliable, high-efficiency performance for energy infrastructure and industrial drive applications.

Renewable energy and high-power industrial applications require a high breakdown voltage (BV), as provided by the 1700 V NTH4L028N170M1 EliteSiC MOSFET. The NTH4L028N170M1 offers a maximum gate-to-source voltage (VGS) range of -15 V to +25 V, making it suitable for fast switching applications where gate voltages are increasing to -10 V, delivering improved system reliability. The 1700 V EliteSiC MOSFET achieves a market-leading gate charge (Qg) of 200 nC at a test condition of 1200 V at 40 Amps. This low Qg enables the device to achieve high efficiency in fast switching, high-power renewable energy applications.

With a BV rating of 1700 V, the NDSH25170A and NDSH10170A EliteSiC Schottky diodes provide an improved margin between the maximum reverse voltage (VRRM) and the peak repetitive reverse voltage of the diode. These devices also allow designers to achieve stable high-voltage operation at elevated temperatures while offering high efficiency enabled by SiC.

Whether it’s an EV charging station, a power grid utilizing renewable energy or high-voltage/high-current industrial drive applications, the onsemi EliteSiC solutions deliver best-in-class efficiency with reduced power losses.

Mouser, the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, launched more than 122,000 new parts in the last two years. To learn more about the onsemi EliteSiC devices, visit https://www.mouser.com/new/onsemi/onsemi-wide-band-sic/.

To learn more about the NTH4L028N170M1 1700 V EliteSiC MOSFET, visit https://www.mouser.com/new/onsemi/onsemi-nth4l028n170m1-mosfet/.

To learn more about the NDSH25170A and NDSH10170A 1700 V EliteSiC Schottky diodes, visit https://www.mouser.com/new/onsemi/on-semi-1700v-diodes/.

 

About onsemi

2026 - onsemi is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end markets, the company is accelerating change across megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world's most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the Nasdaq-100 Index® and S&P 500® index.