New at Mouser: Maxim Integrated MAX25530 LED/TFT Backlight Driver for Automotive Displays

Paskelbti nedelsiant

Susisiekite su mumis


July 8, 2021Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now shipping MAX25530 four-channel automotive backlight driver from Maxim Integrated Products, Inc. The MAX25530 integrates four I²C-controlled, 150 mA LED backlight drivers and a four-output thin-film-transistor liquid-crystal display (TFT-LCD) bias in a single 40-pin, 6 mm × 6 mm chip to help engineers reduce the design footprint of automotive dashboards, central information, and navigation displays.

The Maxim Integrated MAX25530, available from Mouser, integrates one positive boost converter, one negative boost converter, two charge pump drivers for powering up TFT bias, and a boost/SEPIC controller for powering up to four strings of LEDs in the display backlight. For bigger and higher-resolution displays, TFT bias and LED driver are needed. The MAX25530 supports larger screen sizes and higher resolution by providing positive analog supply voltage and negative analog supply voltage, both of which are required for low-temperature polysilicon panels (LTPS) that deliver higher resolution and lower cost than amorphous silicon panels now currently in use.

For design support, Mouser also offers the MAX25530 evaluation kit, a fully assembled and tested surface-mount PCB, that provides a complete power-management solution for automotive displays. The kit can be configured to operate in a standalone mode or in an I²C mode, providing an I²C interface that can operate in conjunction with the MINIQUSB+ adapter board, or a third-party I²C master. The MAX25530 evaluation kit also includes Windows-compatible software that provides a simple graphical user interface (GUI) for exercising the features of the MAX25530 IC.

To learn more about the MAX25530, visit https://www.mouser.com/new/maxim-integrated/maxim-max25530-drivers/.

 

About Maxim Integrated

2026 - Maxim Integrated, an engineer's engineering company, exists to solve the designer's toughest problems in order to empower design Innovation. The company's broad portfolio of high-performance semiconductors, combined with world-class tools and support, delivers essential analog solutions including efficient power, precision measurement, reliable connectivity and robust protection along with intelligent processing. Designers in application areas such as automotive, communications, consumer, data center, healthcare, industrial and IoT trust Maxim to help them quickly develop smaller, smarter and more secure designs. Learn more at https://www.maximintegrated.com.