Mouser-Supported DRAGON / PENSKE AUTOSPORT Team Gears Up for Challenging London E-Prix Street Circuit

Paskelbti nedelsiant

Susisiekite su mumis


June 26, 2022 – Coming off a great qualifying performance in the New York City E-Prix, the Mouser Electronics-backed DRAGON / PENSKE AUTOSPORT Formula E team will head across the pond for the London E-Prix on July 30 and 31. Team drivers Sérgio Sette Câmara and Antonio Giovinazzi will once again contend with a unique indoor/outdoor street course that pits drivers against not just each other but also changing lighting, road surfaces, and serpentine curves surrounding the ExCeL London exhibition center.

Since 2015, Mouser and valued manufacturer Molex have been proud partners of the DRAGON / PENSKE AUTOSPORT team. Joining them for the 2021–22 ABB FIA Formula E World Championship racing season are TTI, Inc. and KYOCERA AVX. Racing is all about speed and endurance, and racing sponsorships are an innovative way for Mouser to communicate its performance-driven business model and promote the newest technologies from its manufacturer partners.

The Formula E series features cars that are powered solely by electricity and represent a vision for the future of the motor sports industry, serving as a framework for research and development around zero-emission motoring. The Gen2 cars offer a huge step forward in electric vehicle racing technology, with maximum power of 250 kW and speeds up to 280 km/h.

Fans can cast a vote for Sette Câmara and Giovinazzi in FANBOOST, which allows fans to play an active role in influencing the outcome of the race. FANBOOST gives fans the opportunity to vote for their favorite driver and award them an extra boost of power during the race. The five drivers with the most FANBOOST votes are awarded a significant burst of power, which they can deploy in a 5-second window during the second half of the race. FANBOOST voting for the London E-Prix opens July 27 and is available up to 15 minutes into the race.

After the weekend doubleheader in London, the series heads to Seoul, South Korea, where the 2021–22 season will come to a close with two races on August 13 and 14.

For more information about Formula E and to register and vote in FANBOOST, visit https://www.mouser.com/formula-e.