Mouser Stocking Espressif Systems ESP32-C6-WROOM-1 Multiprotocol Wi-Fi / Bluetooth Modules for Smart Applications

Pranešimas apie naują produktą

Susisiekite su mumis


October 2, 2023Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now stocking the ESP32-C6-WROOM-1 multiprotocol modules from Espressif Systems. These multiprotocol modules offer a turnkey solution for adding wireless connectivity to applications such as smart homes, industrial automation, health care and consumer electronics.

The Espressif Systems ESP32-C6-WROOM-1 multiprotocol modules, available from Mouser, feature an embedded ESP32-C6 system-on-chip (SoC) powered by a 160MHz 32-bit RISC-V single-core microprocessor, with Wi-Fi® 6 (802.11ax) and Bluetooth® capability, an integrated 40 MHz crystal oscillator and SPI flash up to 8MB. The ESP32-C6-WROOM-1 supports the OFDMA mechanism for both uplink and downlink communications, while also supporting MU-MIMO for downlink traffic, creating high efficiency and low latency, even in congested wireless environments. These multiprotocol modules also enable customers to build Matter-compliant Wi-Fi end-point devices and Thread end-point devices, for interoperability in smart-home devices. The modules also boast 23 general-purpose input and outputs (GPIOs), rich peripherals and on-chip debugging, and are offered with an onboard PCB antenna or with an external antenna connector.

Also available from Mouser, the Espressif Systems ESP32-C6-DevKitC-1 is an entry-level development board based on the ESP32-C6-WROOM-1 module. This development board integrates complete Wi-Fi, Bluetooth LE, Zigbee and thread functions. Most of the I/O pins are broken out to the pin headers on both sides for easy interfacing. Developers can either connect peripherals with jumper wires or mount ESP32-C6-DevKitC-1 on a breadboard. An onboard USB Type-C™ port is used for supplying power to the board, as well as for communication with the ESP32-C6 chip. The ESP32-C6-DevKitC-1 features a USB-to-UART bridge, pin header, status LEDs, and boot and reset buttons for ease of use.

To learn more about the ESP32-C6-WROOM-1 multiprotocol modules, visit https://www.mouser.com/new/espressif/espressif-esp32-c6-wroom-1-modules/.

To learn more about the ESP32-C6-DevKitC-1 development board, visit https://www.mouser.com/new/espressif/espressif-esp32-c6-devkitc-1-board/.

About Espressif Systems

2026 - Espressif Systems is an advanced and professional IC design company that provides low-power Wi-Fi and Bluetooth SoCs and wireless solutions for Internet of Things (IoT) applications. The company has a team of innovators from around the world, working in the areas of chip design, algorithm research, software development, open source development, product development, and customer services.