Now at Mouser: Analog Devices ADMV4540 K-Band Quadrature Demodulator for Satellite Comms

Pranešimas apie naują produktą

Susisiekite su mumis


February 24, 2022Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the ADMV4540 K-band quadrature demodulator from Analog Devices. The ADMV4540 is a highly integrated orthogonal demodulator with a built-in synthesizer that is suitable for next-generation K-band high-throughput, ground terminal satellite communication systems requiring a full outdoor unit.

The Analog Devices ADMV4540 quadrature demodulator, available from Mouser Electronics, is a single-chip solution with a supply voltage of 3.3 V and less than 3.2 W of total power dissipation. The device offers an integrated synthesizer with voltage-controlled oscillator (VCO), downconverter, filtering baseband amplifiers, low-noise amplifier (LNA), and Serial Peripheral Interface (SPI) control capabilities that enable designers to condense their designs into a smaller overall footprint.

The device’s RF front end consists of two LNA paths that allow support for multiple antenna polarizations, with an operating frequency range of 17 GHz to 22 GHz. Each path has an optimal cascaded, 5 dB, double-sideband noise figure at maximum gain, where the LNA path is selectable through the device's programmable 4-wire SPI.

The ADMV4540’s integrated fractional-N phase-locked loop and low-phase-noise VCO generate the necessary on-chip local oscillator signal for the device's two double balanced I/Q mixers to enable the LNA output to downconvert to baseband. The demodulator’s excellent matching between channels and the high spurious-free dynamic range (SFDR) overall gain are well suited for satellite communication systems with dense constellations, multiple carriers, and nearby interferers.

For development, Mouser also stocks the ADMV4540-EVALZ evaluation board, which includes a pre-installed ADMV4540 demodulator and all required external components. The board requires the System Demonstration Platform-Serial (SDP-S) controller board, available separately. 

To learn more about the Analog Devices ADMV4540 quadrature demodulator, visit https://www.mouser.com/new/analog-devices/adi-admv4540-kband-quadrature-demodulator/.

 

About Analog Devices Inc.

2026 - Analog Devices, Inc. is a global semiconductor leader that bridges the physical and digital worlds to enable breakthroughs at the Intelligent Edge. ADI combines analog, digital, and software technologies into solutions that help drive advancements in digitized factories, mobility, and digital healthcare, combat climate change, and reliably connect humans and the world. With revenue of more than $12 billion in FY22 and approximately 25,000 people globally working alongside 125,000 global customers, ADI ensures today’s innovators stay Ahead of What’s Possible.