Mouser Now Stocking Analog Devices AD9081 & AD9082 MxFEs for Broadband Communications and Wide-Bandwidth Signal Processing

Pranešimas apie naują produktą

Susisiekite su mumis


July 22, 2021Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now shipping the AD9081 and AD9082 mixed-signal front-ends (MxFE™) from Analog Devices, Inc. The two versatile RF converter platforms combine high-performance analog and digital signal processing for wireless applications, including 4G LTE and 5G millimeter-wave (mmWave) radios as well as phased array radar systems and electronic defense applications.

The Analog Devices AD9081, available from Mouser Electronics, is a reconfigurable, highly integrated RF MxFE that incorporates four 16-bit, 12 GSPS digital-to-analog (DAC) cores and four 12-bit, 4 GSPS analog-to-digital converter (ADC) cores. Eight transmit and eight receive lanes provide 24.75 Gbps/lane at JESD204C, or 15.5 Gbps/lane at JESD204B. The AD9081 is available in two models: the 4D4AC model supports full instantaneous channel bandwidth, and the 4D4AB model provides maximum fast bandwidth at 600 MHz per channel, with automatic configuration of the digital signal processor (DSP) to limit bandwidth at startup.

The AD9082 MxFE integrates four 16-bit, 12 GSPS DAC cores and two 12-bit, 6 GSPS ADC cores, with support for eight transmit and eight receive lanes, providing 24.75 Gbps/lane (JESD204C) or 15.5 Gbps/lane (JESD204B). The AD9082 is also available in two models — the 4D2AC model, which supports four DACs and two ADCs, and the 2D2AC model, which supports two DACs and two ADCs. Both MxFEs feature an on-chip clock multiplier and DSP and offer a bypass mode to allow the ADC or DAC cores’ full bandwidth capability to bypass DSP data paths.

The AD9801 and AD9802 are supported by the AD9081-FMCA-EBZ and AD9082-FMCA-EBZ evaluation boards, respectively, which include all support circuitry required to operate the MxFEs in various modes and configurations. The eval boards connect to the ADI ADS9-V2EBZ or the ADS8-V3EBZ (sold separately) for evaluation with the ADI Analysis | Control | Evaluation (ACE) software, and can also interface with FPGA development boards from Xilinx® or Intel®.

To learn more about the AD9081 MxFE, visit https://www.mouser.com/new/analog-devices/adi-ad9081-adcs/. For more information about the AD9082 MxFE, go to https://www.mouser.com/new/analog-devices/adi-ad9082-mxfe/.

 

About Analog Devices Inc.

2026 - Analog Devices, Inc. is a global semiconductor leader that bridges the physical and digital worlds to enable breakthroughs at the Intelligent Edge. ADI combines analog, digital, and software technologies into solutions that help drive advancements in digitized factories, mobility, and digital healthcare, combat climate change, and reliably connect humans and the world. With revenue of more than $12 billion in FY22 and approximately 25,000 people globally working alongside 125,000 global customers, ADI ensures today’s innovators stay Ahead of What’s Possible.