Now Available at Mouser: ams OSRAM TMF8820, TMF8821 and TMF8828 Multizone Time-of-Flight Sensors

Pranešimas apie naują produktą

Susisiekite su mumis


March 1, 2022Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, is now offering the TMF8820, TMF8821, and TMF8828 multizone time-of-flight sensors from ams OSRAM. The high-performance direct-time-of-flight (dToF) sensors achieve a 5-meter detection range, while the devices’ multi-lens array significantly widens the field of illumination.

The TMF8820 and TMF8821 sensors, now in stock at Mouser Electronics, and TMF8828 sensor, available to order, are built using single-photon avalanche diode (SPAD) array, time-to-digital converter (TDC), and histogram technology. The sensors feature an associated vertical-cavity surface-emitting laser (VCSEL), while the high-quality lens on the SPAD supports a dynamically adjustable field of view up to 63°. The highly versatile sensors enable detection of the target area in multiple zones with extremely precise measurement results. The sensors can also detect multiple objects per zone, allowing automated robots to gain additional sensory awareness and provide early alerts to potential obstacles.

The TMF8820, TMF8821, and TMF8828 sensors from ams OSRAM perform all raw data processing on chip, and the devices report both distance information and confidence values through an I²C interface. Housed in a single compact modular package, the sensors support a range of demanding applications, including laser detect autofocus for mobile phone cameras, object detection and collision avoidance, presence detection, and light curtain applications for industrial safety designs.

To learn more, visit https://www.mouser.com/new/ams-osram/ams-tmf8820-tmf8821-tmf8828-tof-sensor/.

 

About ams OSRAM

2026 - The ams OSRAM Group is a global leader in optical solutions. By adding intelligence to light and passion to innovation, ams OSRAM enrich people’s lives. This is what they mean by Sensing is Life. With over 110 years of combined history, their core is defined by imagination, deep engineering expertise, and the ability to provide global industrial capacity in sensor and light technologies. They create exciting innovations that enable our customers in the consumer, automotive, healthcare, and industrial sectors to maintain their competitive edge and drive innovation that meaningfully improves the quality of life in terms of health, safety, and convenience, while reducing impact on the environment.

ams is a registered trademark of ams-OSRAM AG. In addition, many of their products and services are registered or filed trademarks of ams OSRAM Group.