New at Mouser: ams OSRAM Mira016 CMOS NIR Image Sensors for Industrial, Robotics and Machine Vision Applications

Pranešimas apie naują produktą

Susisiekite su mumis


March 26, 2025Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now shipping the Mira016 CMOS image sensors from ams OSRAM. The Mira016 image sensor is a compact (0.16MP), enhanced near-infrared (NIR), global shutter image sensor designed for 2D and 3D industrial, robotics, consumer wearables and machine vision applications.

The ams OSRAM Mira016 CMOS image sensor, available from Mouser, is a high sensitivity, small pixel size (2.79 µm) sensor featuring state-of-the-art back-illuminated sensor (BSI) technology. Its small 1.8 mm2 size, configurability, and high sensitivity both in visual as well as NIR wavelengths make the Mira016 well suited for many 2D and 3D applications, including eye, head, hand, and environment tracking in augmented reality and virtual reality (AR/VR).

The Mira016 sensor offers a MIPI CSI-2 interface, allowing easy connection with a variety of processors and FPGAs, and its low active power and high sensitivity in near-infrared (NIR), delivers increased measurement range, as well as overall system power consumption optimization, which is key for battery-powered consumer and industrial applications like facial authentication for mobile devices and points of payment.

Programmable registers, context switching, on-chip processing, advanced power and temperature management, and an illumination synchronization trigger make the Mira016 a perfect choice for authentication, 3D sensing, wearables and extended battery-powered applications.

To learn more, visit https://www.mouser.com/new/ams-osram/ams-osram-mira016-sensor/.

 

About ams OSRAM

2026 - The ams OSRAM Group is a global leader in optical solutions. By adding intelligence to light and passion to innovation, ams OSRAM enrich people’s lives. This is what they mean by Sensing is Life. With over 110 years of combined history, their core is defined by imagination, deep engineering expertise, and the ability to provide global industrial capacity in sensor and light technologies. They create exciting innovations that enable our customers in the consumer, automotive, healthcare, and industrial sectors to maintain their competitive edge and drive innovation that meaningfully improves the quality of life in terms of health, safety, and convenience, while reducing impact on the environment.

ams is a registered trademark of ams-OSRAM AG. In addition, many of their products and services are registered or filed trademarks of ams OSRAM Group.