Mouser Now Shipping ams OSRAM AS5172E High-Resolution Automotive Magnetic Position Sensor

Pranešimas apie naują produktą

Susisiekite su mumis


April 13, 2022Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the AS5172E high-resolution magnetic position sensor from ams OSRAM. With AEC-Q100 Grade 1-qualified construction, the magnetic position sensor offers durable performance for automotive applications including brake and gas pedals, fuel-level measurement systems, steering angle sensors, and contactless potentiometers.

The ams OSRAM AS5172E sensor, available from Mouser Electronics, provides a highly accurate angular position measurement by determining the orthogonal component of the magnetic flux density over a full-turn rotation. Featuring a 14-bit sensor array and analog front end, the sensor uses a differential measurement method to compensate for external stray magnetic fields, ensuring accurate results through a 12-bit PSI5 output (V1.3 and V2.1) at 90° minimum arc.

The highly durable AS5172E sensor supports an extended operating temperature range of -40°C to 125°C and a supply voltage of up to 16.5 V, with overvoltage protection to 20 V and reverse polarity protection to ‑18 V.

To learn more, visit https://www.mouser.com/new/ams-osram/ams-as5172e-magnetic-sensor/.

 

About ams OSRAM

2026 - The ams OSRAM Group is a global leader in optical solutions. By adding intelligence to light and passion to innovation, ams OSRAM enrich people’s lives. This is what they mean by Sensing is Life. With over 110 years of combined history, their core is defined by imagination, deep engineering expertise, and the ability to provide global industrial capacity in sensor and light technologies. They create exciting innovations that enable our customers in the consumer, automotive, healthcare, and industrial sectors to maintain their competitive edge and drive innovation that meaningfully improves the quality of life in terms of health, safety, and convenience, while reducing impact on the environment.

ams is a registered trademark of ams-OSRAM AG. In addition, many of their products and services are registered or filed trademarks of ams OSRAM Group.