Mouser Electronics Now Stocking Xilinx Spartan-7 I/O-Intensive FPGAs

Pranešimas apie naują produktą

Susisiekite su mumis


Mouser Electronics Now Stocking Xilinx Spartan-7 I/O-Intensive FPGAs

November 25, 2019 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking Spartan®-7 field programmable gate arrays (FPGAs) from Xilinx.

Xilinx Spartan-7 FPGAs feature a MicroBlaze™ soft processor running over 200 DMIPs with 800 Mbit per second DDR3 support built on 28nm technology. FPGAs are semiconductor devices that are based around a matrix of configurable logic blocks (CLBs) connected via programmable interconnects. The Spartan-7 offer integrated analog-to-digital converters, dedicated security features, and Q-grade (-40 to +125°C) on all commercial devices. Spartan-7 devices enable key connectivity and processing applications in industrial, automotive, consumer, and communications markets. Spartan-7 is among four FPGA families (Virtex-7, Artix-7, and Kintex-7 are the others) that address system requirements ranging from small form factor, cost-sensitive, high-volume applications to ultra high-end connectivity bandwidth, logic capacity, and signal-processing capability.

Applications for the Spartan-7 field programmable gate arrays include machine vision interfacing, single-axis motor control, cryptographic engine for V2X applications, adaptive LED lighting system, and automotive data format/standard conversion.

To learn more, visit https://www.mouser.com/new/xilinx/xilinx-spartan-7-fpga/.

With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

Apie AMD / Xilinx

2026 - AMD / Xilinx develops highly flexible and adaptive processing platforms that enable rapid innovation across a variety of technologies, from the endpoint to the edge to the cloud. Specializing in programmable logic devices, Xilinx is the semiconductor company that invented the Field Programmable Gate Array (FPGA), the hardware programmable System on Chip (SoC), and the Adaptive Compute Acceleration Platform (ACAP).