Mouser Now Stocking SparkFun Artemis Dev Kit with Full Arduino, Bluetooth, and Mbed Support

Pranešimas apie naują produktą

Susisiekite su mumis


Mouser Now Stocking SparkFun Artemis Dev Kit with Full Arduino, Bluetooth, and Mbed Support

October 15, 2020 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the Artemis Development Kit with Camera from SparkFun.

SparkFun Artemis Development Kit with Camera is the latest board to be released around the SparkFun Artemis Module, and it allows access to more software development features than previous Artemis based boards. Recommended software used to program the Artemis Development Kit are the Arduino IDE, Arm® Mbed™ OS (Studio and CLI), and AmbiqSDK. An updated USB interface (NXP MKL26Z128VFM4 Arm Cortex®-M0+ microcontroller) allows the SparkFun Artemis Development Kit to act as mass storage device (MSD), human interface device (HID), and communication port (COM).

The Artemis Module includes a 48-MHz Arm Cortex-M4F processor with an available 96MHz turbo mode. The Cortex core includes with Bluetooth Low Energy 5.0 connectivity and offers low power consumption down to 6 µA per MHz (less than 5 mW). The SparkFun Artemis Module is fully FCC/IC/CE certified with 1 Mbyte of flash and 384 Kbytes of RAM that gives plenty of room for the user's code. The flexibility of the Artemis module starts with an Arduino core. The user can program and use the Artemis module just like they would an Uno or any other Arduino board. Additional functionality stems from the ability of the Artemis Development Kit to run a real-time operating system (RTOS) such as the Arm Mbed OS or the AmbiqSDK.

Attached to the Qwiic I2C bus is a LIS2DH12TR MEMS accelerometer (for gesture recognition) and a digital MEMS microphone. It also includes an edge camera connector for the Himax CMOS imaging camera to experiment with always-on voice commands and image recognition with TensorFlow and machine learning.

To learn more about the SparkFun Artemis Development Kit with Camera, visit https://www.mouser.com/new/sparkfun/sparkfun-kit-17071-artemis-development-kit/.

Apie SparkFun

2026 - As a manufacturer and proponent of open-source hardware, SparkFun has been helping turn ideas into reality since 2003. Whether you’re creating a smart weather station, exploring the frontier of machine learning, or prototyping a product, SparkFun’s ever-growing catalog has the products and resources you need to start something.