Mouser Electronics Now Stocking Littelfuse LS0502SCD33 Supercapacitor Protection IC for Backup Power Charging
March 7, 2024 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the Littelfuse LS0502SCD33 supercapacitor protection IC from Littelfuse.
The Littelfuse LS0502SCD33 supercapacitor protection IC, available from Mouser, is a complete solution for systems with a backup storage capacitor or a capacitor bank. Littelfuse LS0502SCD33 Supercapacitor IC integrates input overvoltage protection, an overcurrent protection circuit, a reverse blocking switch, and a supercapacitor charging control circuit. This protection device for backup power also has a built-in cell balance to protect a two-cell supercapacitor system. When the main supply is present and above the minimum system supply voltage, the system draws power from the input supply. An integrated linear charger charges the storage element at up to 300mA current. When the storage element is charged, the circuit draws just 2.5μA current while maintaining the supercapacitor or other storage element in its ready state. When the main supply is removed, the integrated reverse blocking switch blocks current flow from the system rail to the input.
The linear charger is turned on to provide power to the system rail with a low resistance path featuring up to 2A current. The integrated cell balancing circuit monitors the cell voltage when charging and keeps the voltage of the two cells at the same level. A user can externally program the Littelfuse LS0502SCD33 for input current limit, input overvoltage, charge current limit, and charge voltage limit. This protection IC provides a flag signal when the input supply is unplugged so that the primary system can take action.
Applications for the LS0502SCD33 include handheld industrial equipment, dash cameras, IoT, smart meters, and portable devices with removable batteries.
To learn more, visit https://www.mouser.com/new/littelfuse/littelfuse-ls0502scd33-super-capacitor-ic/.
2026 - Littelfuse is an industrial technology manufacturing company empowering a sustainable, connected, and safer world. Across more than 15 countries, and with 17,000 global associates, Littelfuse partners with customers to design and deliver innovative, reliable solutions. Serving over 100,000 end customers, Littelfuse products are found in a variety of industrial, transportation and electronics end markets – everywhere, every day.