Mouser Electronics Now Shipping ams OSRAM FIREFLY® E1608 CH DELSS1.22 LED
January 12, 2023 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the FIREFLY® E1608 CH DELSS1.22 LED from ams OSRAM.
The ams OSRAM FIREFLY® E1608 CH DELSS1.22 Light Emitting Diode (LED) is designed specifically for SpO2 applications. This hyper-red CH DELSS1.22 LED features a special narrow wavelength of 665 nm to improve signal detection, thin film chip technology, and 120° typical radiation (Lambertian emitter). The FIREFLY E1608 LED operates between -40°C to +85°C temperature range and is available in a compact 0.8 mm x 1.6 mm x 0.6 mm package, ideal for space-constrained designs.
Applications for the FIREFLY E1608 LED include SpO2 applications, health monitoring, heart rate monitoring, pulse oximetry, and fitness tracking.
To learn more, visit https://www.mouser.com/new/ams-osram/osram-firefly-e1608-ch-delss1-22-led/.
2026 - The ams OSRAM Group is a global leader in optical solutions. By adding intelligence to light and passion to innovation, ams OSRAM enrich people’s lives. This is what they mean by Sensing is Life. With over 110 years of combined history, their core is defined by imagination, deep engineering expertise, and the ability to provide global industrial capacity in sensor and light technologies. They create exciting innovations that enable our customers in the consumer, automotive, healthcare, and industrial sectors to maintain their competitive edge and drive innovation that meaningfully improves the quality of life in terms of health, safety, and convenience, while reducing impact on the environment.
ams is a registered trademark of ams-OSRAM AG. In addition, many of their products and services are registered or filed trademarks of ams OSRAM Group.