Maxim Integrated MAX78002 Artificial Intelligence Microcontroller Now Shipping from Mouser

Glaustas pranešimas žiniasklaidai apie naują produktą

Susisiekite su mumis


March 31, 2023 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the MAX78002 Artificial Intelligence (AI) microcontroller from Maxim Integrated.

The Maxim Integrated MAX78002 is an AI microcontroller optimized to enable neural networks to execute
at ultra-low power and live at the edge of the Internet of Things (IoT). The device combines energy-efficient AI processing with an ultra-low-power design. This hardware-based CNN accelerator enables battery-powered applications to execute AI inferences while expending only millijoules of energy.

The MAX78002 is an advanced system-on-chip featuring an Arm® Cortex®-M4 with FPU CPU for efficient system control with an ultra-low-power deep neural network accelerator. The CNN engine has a weight storage memory of 2 MB and can support 1-, 2-, 4-, and 8-bit weights (supporting networks of up to 16 million weights). The CNN weight memory is SRAM-based so that AI network updates can be made on the fly. The CNN engine also has 1.3 MB of data memory. The CNN architecture is highly flexible, allowing networks to be trained in conventional toolsets like PyTorch® and TensorFlow®, then converted for execution on the MAX78002 using tools provided by Analog Devices. The device is supported by the MAX78002 evaluation kit, also available from Mouser Electronics.

Applications for the MAX78002 Artificial Intelligence microcontroller include factory robot and drone navigation, industrial sensors and process control, inline quality assurance vision systems, smart security cameras and portable medical diagnostics equipment.

To learn more, visit https://www.mouser.com/new/maxim-integrated/maxim-max78002-microcontrollers/.

 

About Maxim Integrated

2026 - Maxim Integrated, an engineer's engineering company, exists to solve the designer's toughest problems in order to empower design Innovation. The company's broad portfolio of high-performance semiconductors, combined with world-class tools and support, delivers essential analog solutions including efficient power, precision measurement, reliable connectivity and robust protection along with intelligent processing. Designers in application areas such as automotive, communications, consumer, data center, healthcare, industrial and IoT trust Maxim to help them quickly develop smaller, smarter and more secure designs. Learn more at https://www.maximintegrated.com.