Murata Power Supply Line Noise Suppression for Home Audio

Digital amplifiers are increasingly popular for home audio applications. In many cases, power is supplied from an AC outlet for home audio, and the conductive noise in the power supply cable is regulated under EMC standards. Therefore, it is necessary to prevent noise from leaking into the power supply line during audio playback. Here is an overview of noise problems in home audio cables and their solutions.

Impact of the Power Supply & Countermeasures

The quality of the power supply is important to output superior audio from an audio device. Figure 1 (below) shows the THD + N results when another device is connected to the power supply outlet of a home audio device. While the THD + N deteriorates across the entire audible range when suppression is not implemented in the power supply line, applying suppression improves the THD + N result and the audio quality (Figure 2, below).

Murata's PLT10HH Large Current Common Mode Choke Coils and BNX block-type EMIFIL® filters are effective for providing suppression from low to high frequencies in power supply lines. Both series are ideally suited for use in various sets to suppress power supply noise.

Figure 1

Murata Power Supply Line Noise Suppression for Home Audio

Example of noise interference from power supply circuits and countermeasures

Figure 2

Murata Power Supply Line Noise Suppression for Home Audio

Audio quality measurement results with power supply circuit suppression

Impact of Audio Circuits & Countermeasures

An AC outlet typically provides power to home audio applications. The conductive noise in the power supply cable is regulated under EMC standards, making it necessary to prevent noise from leaking into the power supply line during audio playback.

Methods of cutting the noise are generally introduced into the AC adapter or the AC-DC power supply section. However, it is easier to avoid the noise issue by applying suppression in the power supply section of the digital amplifier that is the source of the noise (Figure 3, below).

Figure 4 (below) illustrates the results of measuring the noise leaking from the power supply line. It shows the higher harmonics of the digital amplifier switching frequencies are conducted as noise. Equipping Murata PLT10HH choke coils and BNX filters achieved an improvement of more than 20dB.

Using both series enables designers to suppress noise interference from the power supply circuit to the audio equipment as well as suppress noise leaking from the audio equipment to the power supply.

Figure 3

Murata Power Supply Line Noise Suppression for Home Audio

Example of countermeasures to deal with noise leakage from a Class D amplifier to the power supply circuit

Figure 4

Murata Power Supply Line Noise Suppression for Home Audio

Power supply noise measurement results before and after applying suppression products

Community Forum

Murata Community Forum provides searchable content with various discussion topics, popular blogs, and articles. The Murata broad market support team holds regular reviews to discuss open issues, allowing inquiries to be answered in a timely manner. The forum content is freely accessible to the public. However, users must log in to post questions or answers. Registration is free of charge.

Paskelbta: 2021-01-22 | Atnaujinta: 2022-03-11