Lattice MachXO3 FPGAs with Very High Density I/O Available from Mouser

Paskelbti nedelsiant

Susisiekite su mumis


Lattice MachXO3 FPGAs with Very High Density I/O Available from Mouser

July 14, 2014 - Mouser Electronics, Inc. is now stocking the MachXO3™ Field Programmable Gate Arrays (FPGAs) from Lattice Semiconductor. The MachXO3 uses a new packaging technology that eliminates bond wires, both increasing performance while reducing cost. This innovative packaging approach results in increased gate and input/output (I/O) density while maintaining a small board footprint. The MachXO3 FPGAs are designed on a 65nm non‑volatile low power process technology and operate as fast as 150MHz.

The new Lattice Semiconductor MachXO3 Field Programmable Gate Arrays, available from Mouser Electronics, boast a very high gate density not usually found in programmable logic. These FPGAs feature low power consumption with almost instant-on activity after power-up. Densities in this FPGA family range from 640 to 6900 Look-Up Tables (LUTs). In addition to LUT-based low-cost programmable logic these devices also feature embedded block RAM (EBR) and distributed RAM. Internal phase locked loops (PLLs) reduce component count.

Advanced configuration support includes dual-boot capability and hardware versions of commonly used embedded blocks such as an SPI interface, two I2C interfaces, and a timer/counter. These features allow developers to quickly configure these devices for their applications without having to configure the FPGA for these commonly used logic blocks.

Enhanced flexibility in the I/O include drive strength control for driving external loads, slew rate control to compensate against high frequency oscillations, PCI bus compatibility, internal pull‑up and pull‑down resistors on the I/O pins, and open drain outputs for driving loads.

The MachXO3 is flexible enough to be used across many market segments including consumer, communications, data storage, industrial applications, and automotive applications.

To learn more, visit:
http://www.mouser.com/new/Lattice-Semiconductor/lattice-machxo3-fpgas/ .

With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 20 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

About Lattice Semiconductor

2026 - Lattice Semiconductor is the low-power programmable leader, solving customer problems across the network, from the Edge to the Cloud, in the growing communications, computing, industrial, automotive, and consumer markets. Through differentiated low-power, small-sized programmable logic products and related solutions, long-standing relationships, and commitment to world-class support, Lattice enables its customers to quickly and easily unleash their innovation to create a smart, secure, and connected world. In addition to innovative FPGAs, Lattice provides customers with a comprehensive support ecosystem that includes powerful, easy-to-use design tools, IP cores, reference designs, development kits, and local technical support.