Elektroniniai komponentai
Užbėkite įvykiams už akių
Pramonės automatika
Pramoninė automatika – viskas po ranka
(Source: Olivier Le Moal/stock.adobe.com)
As digital systems grow more interconnected, the traditional boundaries of cybersecurity have all but disappeared. From cloud platforms and remote endpoints to smart devices and operational technology, the need for a new security model has become urgent. Today, the modern network is a sprawling, dynamic environment—one where implicit trust is no longer part of a viable defense plan.
This shift has propelled Zero Trust Architecture (ZTA) to the forefront of cybersecurity strategy. Rather than relying on outdated perimeter-based models, ZTA assumes that no user or device should be trusted by default, regardless of where they’re located.[1] It’s a model built for the realities of today’s threat landscape—where breaches are inevitable and resilience depends on constant verification and adaptive control.
This blog explores the architectural foundation of Zero Trust, breaking down its core components and explaining how they work together to create a more resilient security posture.
For decades, cybersecurity operated like a medieval fortress. Firewalls and VPNs formed the moat, and once you were inside, you were trusted. But in today’s world, where remote work, cloud computing, and Internet of Things (IoT) devices are the norm, that model is dangerously outdated.
Take a modern factory, for example. Hundreds of sensors stream data to the cloud. Engineers log in from home. Vendors access systems off-site for maintenance. In this environment, there’s no clear “inside” or “outside.” Every connection is a potential vulnerability.
Zero Trust flips the script. Instead of assuming trust based on location, it verifies every user and device—every time.
The first pillar of Zero Trust is identity—knowing exactly who or what is requesting access. In traditional models, being inside the network often meant automatic trust. But ZTA demands continuous verification, even for users and devices that have already been authenticated.
This process typically starts with identity providers (IdPs) and multi-factor authentication (MFA), which confirm a user’s credentials. But identity alone isn’t enough. Devices must also meet security standards, such as having up-to-date patches or antivirus protection, before they’re granted access. These posture checks ensure that even trusted users can’t introduce risk through vulnerable endpoints.
Think of it like airport security: showing your ID gets you through the first checkpoint, but your luggage still needs to be scanned. In ZTA, both the traveler and their gear must be cleared before proceeding.
Once identity is established, the next architectural layer comes into play: access enforcement. This is where policy engines evaluate each request in real time, determining what resources a user or device can access and under what conditions.
These decisions are made by policy decision points (PDPs), which apply predefined rules based on roles, time of day, device health, and more. Policy enforcement points (PEPs) then act on those decisions, allowing or denying access accordingly.
For example, a technician might be permitted to update a control system from a company-issued laptop during business hours—but not from a personal device at midnight. This level of granularity is made possible by tools like software-defined perimeters (SDPs), which create encrypted tunnels to specific resources rather than exposing entire networks like traditional VPNs.
In essence, ZTA replaces the “all-access pass” with a “need-to-know” badge that’s constantly reevaluated.
The third architectural pillar is continuous monitoring. In a Zero Trust environment, granting access is just the beginning. Systems must constantly assess whether conditions remain safe, using tools like security information and event management (SIEM) platforms and user and entity behavior analytics (UEBA).
These systems look for anomalies—such as unusual login times, large file transfers, or changes in device position—and respond dynamically. A user downloading sensitive data outside normal hours might be prompted for re-authentication or temporarily restricted until the behavior is verified.
This ongoing vigilance transforms cybersecurity from a static gatekeeper into a dynamic guardian, always watching for signs of trouble and ready to adapt.
While identity, access, and monitoring form the core of ZTA, micro-segmentation adds another layer of protection. By dividing networks into smaller, isolated zones, organizations can limit the spread of breaches.[2] If one segment is compromised, attackers can’t easily move laterally to other systems.
In industrial environments, this might mean separating quality control systems from production machinery. Even if a vulnerability is exploited in one area, the rest of the operation remains secure.
Micro-segmentation is like installing fire doors in a building. A fire in one room doesn’t engulf the entire structure—it’s contained, giving responders time to act.
Another key concept embedded in ZTA is least privilege access. Users and devices are granted only the permissions they need to perform their tasks—nothing more. This minimizes the potential damage from compromised credentials or insider threats.
For instance, an accounting employee doesn’t need access to engineering servers, and a maintenance technician shouldn’t be able to view HR records. By enforcing strict boundaries, ZTA reduces the attack surface and limits the fallout from security incidents.
Zero Trust Architecture isn’t a single product or plug-and-play solution. It’s a strategic framework that requires thoughtful implementation, cross-functional collaboration, and a shift in mindset. But the payoff is significant: a security model that adapts to modern threats, protects critical assets, and empowers organizations to operate with confidence in a connected world.
For engineers, IT professionals, and even everyday users, embracing Zero Trust means taking a proactive stance on security. It’s about building systems that are resilient, adaptable, and ready for whatever comes next.
For a deeper dive into this topic, read the full article, “Why Zero Trust Architecture Is the New Cybersecurity Standard.”
This blog was generated with assistance from Copilot for Microsoft 365.
[1] https://www.crowdstrike.com/en-us/cybersecurity-101/zero-trust-security/ [2] https://arxiv.org/pdf/2501.06281
Mouser Electronics, founded in 1964, is a globally authorized distributor of semiconductors and electronic components for over 1,200 industry-leading manufacturer brands. We specialize in the rapid introduction of the newest products and technologies targeting the design engineer and buyer communities. Mouser has 28 offices located around the globe. We conduct business in 23 different languages and 34 currencies. Our global distribution center is equipped with state-of-the-art wireless warehouse management systems that enable us to process orders 24/7, and deliver nearly perfect pick-and-ship operations.