Phoenix Contact CONTACTRON Hybrid Motor Starters Phoenix has made the following changes to their family of CONTACTRON Hybrid Motor Starters: In the event of a pending control signal, two or three missing phases are now detected e.g., when a fuse blows and also when a motor is not connected. As soon as no current flows on at least one phase after activation or the motor current is lower than the current to be parameterized, the module reports a phase failure in the form of an LED error code as well as via the reply relay. The power path is not switched off in this case. Further information can be found at www.phoenixcontact.com. The new modules can be identified by the data code from CW38/12. Depending on Mouser inventory, both old and new versions of these motor starters may be supplied upon shipment. Part Numbers affected 651-2900414 651-2900692 651-2900421 651-2900542 651-2900422 651-2900543 651-2900544 651-2900545 651-2900546 651-2900550 651-2900552 651-2900553 651-2900554 651-2900555 651-2900558 651-2900559 651-2900560 651-2900561 651-2900562 651-2900566 651-2900567 651-2900568 651-2900569 651-2900570 651-2900573 651-2900574 651-2900575 651-2900576 651-2900578 651-2900582 651-2900685 651-2900686 651-2900688 651-2900689 651-2900691 651-2900420 Please contact a Mouser Technical Sales Representative for further information. 5-0413-20